This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2841: LM2841 repeatedly failing with smoke

Part Number: LM2841

Hi,

I just had the third one of these (LM2841XMK-ADJL) blowing up in my application, and I am failing to find the root cause.

It should not be an overvoltage situation, as there is a 28V SMBJ suppressor diode on the input. The capacitive load at the output of the converter is approx 20uF, and current draw is only some tens of mA. I hope that someone can check my design. Here is the schematic:

Cheers

Frank