This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tidu789c Having startup issues with UCC2877 flyback

Other Parts Discussed in Thread: UCC28722

Having startup issues with UCC2877 flyback

Perhaps this question is best directed at the authors of the application not for the circuit tidu789c 230-V, 400-W, 92% High Efficiency Battery Charger With PFC and LLC for 36-V Power Tools Reference Design.  The authors are listed as SALIL CHELLAPPAN and LATIF AMEER BABU.

 

This circuit is a PFC stage that powers an LLC battery charger.  The flyback that powers it all refuses to startup on the two new circuits.  I believe this is due to the way the circuit is being powered up as per the text from the TI note that  is after my signature.  Note that I have read the recommended troubleshooting information located at file Trouble shooting startup for TI PSR controllers and switchers.pdf with hyperlink /cfs-file/__key/communityserver-discussions-components-files/196/2705.Trouble-shooting-startup-for-TI-PSR-controllers-and-switchers.pdf  The original TI parts are on this board.  The only difference is in the amount of resistance in the trickle charge.  Here is the synopsis of what took place; see the text inside these {brackets}  {The circuit arrived DOA.  I have done everything I can to coax it to start within the specified current levels to no avail.  The part is shorted at pin 2.  The UCC28722 data sheet calls for a 25V zener protection diode at U2 and this is absent from the test board and schematic so it was never included in the first place.  I was suspicious of it when I did the mathematical analysis as to why they didn't clamp that pin voltage.  That 25V zener is only necessary if the startup resistors allow too much current into the part.  I don't see how that could have happened as the resistors are of adequate value and the input voltage only made it to 165V peak instead of the 400V the PFC would produce once it was up and running.  I tried to start a second board at 330 V peak and still, no luck  The flyback wouldn’t produce a secondary voltage as it only clamped to 13V.  Note the resistors on the board are 1.69 MEG and not the specified 3.32 MEG in the LLC/PFC/battery charge schematic.  Again, this shouldn't matter as the current produced is within the specified amount to start the UCC28877 controller without exceeding the rated value for the part which I believe is 16 mA however I don’t have that file open right now.}

 

Based on the startup information, 175V-250 VAC is needed in order to start.  I have put up to 240 VAC into the circuit and it has failed to start.  I believe it is because the TI text states to "Gradually increase the input voltage from 0 V to turn on voltage of 175-V AC".  I don't have the equipment to perform a slow start of this specific nature so this may be the problem. 

 

In a way, it's a good thing I found this out because it will cause problems for your customers who "hot plug" the fixture into the wall.  I may have to design an additional slow start circuit.  In order to find out which of the 3 controllers [LLC/flyback/PFC] is in need of slow starting, I would have to talk to the author of the LLC application note further to find out why a slow start is needed and also find out how slow should it be timewise.  This would be crucial to designing a slow start circuit as I might use a pass element that would overheat if standing off voltage while passing current.

 

Sincerely,

Scott Deuty

970 215 8051

 

 

 

The flyback VCC pin 2 of controller UC28722 is clamping to 13V so I think there is voltage enough to start the flyback however the UVLO specs in the attached graphic indicate otherwise as shown in this text excerpt.

 

*****************Begin UCC28772 data sheet excerpt******************

UNDERVOLTAGE LOCKOUT

VVDD(on) VDD turn-on threshold VVDD low to high 19 21 23

V

VVDD(off) VDD turn-off threshold VVDD high to low 7.2 7.7 8.3

*****************Begin UCC28772 data sheet excerpt******************

 

The lack of 19 volts to start the circuit COULD be the problem however there is 

 

Scott

 

**************Excerpted text from Texas Instruments board document for the LLC tidu789c 230-V, 400-W, 92% High Efficiency Battery Charger With PFC and LLC for 36-V Power Tools Reference Design********

6 Getting Started Hardware

 

6.1 Test Conditions

Input conditions:

• VIN: 175-V to 265-V AC

• Set the input current limit to 3.5 A

Output:

• Variable simulated battery load, 20 to 42 V, 0 to 9 A

6.2 Equipment Needed

• Isolated AC source

• Single-phase power analyzer

• Digital oscilloscope

• Multi-meters

• Electronic load to simulate battery

6.3 Procedure

1. Connect input terminals (connector J1) of the reference board to the AC power source.

2. Connect output terminals (connector J3) to electronic load, maintaining correct polarity.

3. Set the minimum load of about 100 mA, and minimum voltage of 25 V.

4. Gradually increase the input voltage from 0 V to turn on voltage of 175-V AC.

5. Turn on the load to apply voltage to the output terminals of the charger.

6. Observe the startup conditions for smooth switching waveforms.

 

 

**************End of excerpted text from Texas Instruments board document for the LLC tidu789c 230-V, 400-W, 92% High Efficiency Battery Charger With PFC and LLC for 36-V Power Tools Reference Design********

 

  • Scott,

    Thanks for your interest in TI here.

    Can you confirm a few things to help understand your situation here?

    1) how did you have hardware built? Did you provide our TIDA Gerber files and BOM and have a local board house build some for you or did you do your own design based in part on this reference design?

    2) are ALL components the same exact part numbers and values as the ref design BOM or any alternatives? It sounds like you channged some resistors and removed a clamp can you be more specific about what you used and which component reference designators you are referring to? From your comments it sounds like pin2 was damaged so the trickle charge resistor change could have impacted that. Any specific reason you did not copy the reference design exactly?

    3) do you have the capability to follow the test procedure how it explains to properly startup?

    4) were you probing anything during startup? If so can you explain what you were looking at and how you were connected?

    5) this is a large complicated board. In one hand you could replace the ucc28722 IC and try to debug and replace other components but you may have further issues if there were components damaged that you don't find and replace. Sometimes we call a board like that "walking dead" because it may seem to get powered up again but could behave strangely because of some unknown issues from damage. As such you may consider tossing that board into your nearest electronics recycling bin and starting fresh with a new board.

    Regards

    John

  • I got the board from a client. I believe they bought it through TI. As I said, the startup resistors are a higher value on the board than on the schematic. I'm starting it by hot plugging it into 240VAC as 120 VAC is only getting to 165V DC when rectified and going through the PFC inductor and boost diode. The app note calls for 175 min. This will have to be resolved too because the end application needs to hot plug into 120 VAC.
  • Scott,
    If I were you I would use the design files and BOM online and have your own boards built up to match the reference design exactly. That way you know exactly what you're working with. You may also considering disconnecting the flyback and LLC portion to make sure the PFC is working properly, then connecting in/populating the flyback , etc.

    Regards
    John
  • Hello Scott,

    There are several issues to address here, and I’d like to start with the “gradual increase” of input voltage versus “hot plug” into 240Vac.

    This TIDA-00355 design is fully capable of being hot-plugged into a 240Vac line without damage, provided that it is working in the first place. TI generally does not provide reference-design boards directly, but provides the schematic and pcb design files for customers to be able to recreate them. The user guide (TIDU789C) recommends gradual increase of input voltage because a customer-constructed board may have inadvertent bugs in it that a slow increase in voltage may reveal a problem before damage is done that a sudden hot-plug into high voltage could not avoid. This is generally a good practice for any design that has not already been tested and working.

    You have received a board from a client and it is not clear what issues your client had with it, or why the start-up resistor values are lower. (Perhaps the values were cut roughly in half in anticipation of normal running at 120V instead of 240Vac.) In your posting you made two statements: 1. that pin 2 of UCC28722 was “shorted” (it is unclear to what it is shorted), and 2. that on a second board, VCC pin 2 was clamped to 13V. It is possible that both boards were already damaged when you obtained them.

    The voltage at VCC (pin 2) must rise to 21V before the UCC28722 will start switching. If pin 2 is shorted to GND, the IC or the VCC cap is damaged and must be replaced with good parts. On the 2nd board, being clamped to 13V indicates that the D21 diode is not blocking and the start current is running though Zener-clamp D19. This 15-V Zener is likely operating around 13V with the micro-amp level of current available. So, on the second board, I recommend to check D21 as well as U8 and C52 for damage, and replace as necessary.

    I recommend changing R49, R53 and R57 back to 3.3Meg each as the original design calls for. Before startup, the UCC28722 only draws ~1uA at VCC, so even 31Vdc on B+ can provide that much current through ~10Meg by the time VCC got up to 21V. Because of tolerances, higher voltage is advised, but the point is that 240Vac or even 120Vac is not necessary to start the Aux supply controller. Section 5.3 of the User Guide indicates that the Aux supply should regulate with a minimum of 100V on the bulk rail. This corresponds to the peak of ~70Vac. It will attempt to start up with input voltages below 70Vac, but may not stay running or may not regulate properly. All this pre-supposes, of course, that there are no problems with the board(s) in the first place.

    With 3x1.69Meg at R49, R53 and R57, the current to VCC when the system is running comes from a PFC output at ~400V. Istart = (400V-13V)/5.07M = 76uA. This current is much less than the 2mA that IC alone draws (even neglecting Q8 base current) when the system is charging a battery, but in stand-by condition, the Aux load is turned off, and the UCC28722 operates most of the time in a Wait state. In this state, Iwait at VCC is typically 95uA. If the IC requires less than typical wait-state current, or more likely, if there is a leakage path around the resistors (due to pcb surface contamination with flux or moisture) the current into VCC could exceed what the IC requires and VCC will rise above the absolute maximum rating of the device and damage it. This is not the situation where a Zener clamp on VCC is recommended in the datasheet, but it is another situation where such a clamp might be a good idea, although higher resistor values and a clean surface would avoid this.

    So, I recommend that the Auxiliary power stage of both boards be thoroughly inspected and tested at low input voltage so that you are satisfied that it works correctly. I recommend to add a 68-ohm 5-W resistive load across C48 (6V5 output) to do this, to avoid having to deal with any of the other system outputs. Once the Aux supply works, the rest of the board can be powered up, hopefully without requiring additional debug. Conversely, you can remove R49 and Q8, and provide external sources for 6V5 and 13V to power up and test the rest of the system (temporarily) without a working Aux stage.

    It may not be clear, but this TIDA design requires a battery or battery-emulator load to get the PFC and LLC stages to power up. Wen plugged in, the Aux stage operates all the time. It will be in stand-by mode when no battery or battery-load is applied, and bias power to the PFC and LLC stages is shut off to keep total stand-by power low. In order for the PFC and LLC to get bias power (VCC1 and VCC2), the signal LS must be high enough to turn on Q9, which then drives switches for the other bias voltages.

    The signal LS is derived from the sense-resistor string on the main battery charging output. The User Guide indicates that the charger is applicable for 20V-42V battery voltages, so an external voltage of at least 20V must be applied to J3 output in order to activate the PFC and LLC stages. Do not use a bench supply for this purpose because most power supplies are not capable of sinking current (absorbing power). A battery-emulator or a real battery with suitable safeguards should be used.

    Finally, you indicate that the eventual goal is to operate at 120Vac. If you intend to be able to operate at 120Vac in addition to 240Vac, then the PFC stage will need to be redesigned to handle the higher current at the lower voltage, but the LLC stage can stay the same. If you intend to be able to operate at 120Vac instead of 240Vac, then the PFC stage will need to be redesigned to handle the higher current at the lower voltage but stay at 400V output and LLC need not change, OR change the PFC output down to 200V and also change LLC stage for 200V bulk voltage. This can improve the low-line efficiency. In either case, I recommend to follow the design procedures in the respective datasheets rather than that in the TIDA-0355 User Guide, because the guide design descriptions may not have included every possible consideration that the datasheets may mention.

    Good luck with your debug. Please indicate whether this answers your questions and concerns.

    Regards,
    Ulrich

  • Ulrich,

    Thank you for the detailed response.  I shall inspect the board as per your recommendations.  I do appreciate the amount of effort that you put into this response as I was an applicaitons engineer and understand how demanding it can be time wise.  Hoping for a happy ending so I can write a piece on this circuit at my Planet Analog blog.

    Scott Deuty