We have used TPS6112 in one of our prototype designs . Now we need to mak this compliant to EFT ( EN 6100-4-4) 1KV/Leve2 and Surge test(EN 6100-4-5) at 05KV(L-L)/1KV (L-PE).
Does any one have a time tested circuit for fixing this?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We have used TPS6112 in one of our prototype designs . Now we need to mak this compliant to EFT ( EN 6100-4-4) 1KV/Leve2 and Surge test(EN 6100-4-5) at 05KV(L-L)/1KV (L-PE).
Does any one have a time tested circuit for fixing this?
The TPS62110 meets standard 4kV human body model (HBM), 1.5kV charge device model (CDM), and 100V machine model. If additional ESD protection is needed, refer to Texas Instruments' ESD protection devices http://focus.ti.com/paramsearch/docs/parametricsearch.tsp?family=analog&familyId=1441&uiTemplateId=NODE_STRY_PGE_T for an economical solution.