Hi,
There is an question from customer side. The output voltage is not requlated normally when EN pin is tied to the external voltage 18V. In the D/S, the absolute max. voltage can be up to 20V. So it means that the voltage level should be ok with 18V. But we found that the output voltage goes down to 7.5V (Conditions: Vin=12V, Vout=9V for panel Half AVDD application)
PS: For power sequence design, to supply an external voltage to EN pin to make proper sequence for system requirement.
Could you kindly let us know what happened on this IC when supply a 18V to EN pin?
In the D/S, it shows that the total current into the ENABLE pin is limited to no more than 500 uA. Why? If the current is great than 500uA, what happened?
This is urgent case for my major customer, pls kindly help to support this asap, Very thanks.
TI FAE
Brian Wang