This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63060: I'm looking for a Voltage Regulator with similar funcionality, but 15A of output current.

Part Number: TPS63060


Since I want to use a similar device for controlling an Supply Voltage for a Laser with max. efficiency, I would like to have a similar functionality to the TPS63060, where a feedback pin allows for a control. I'd like a supply of 5V for the device in question, output voltage should be higher than 3.3V, and the output current should reach 15A.

Any known devices in your portfolio that might do the trick? I'm thinking of a Buck-Converter of some sort.

Thank you in advance.

André Fernandes