Other Parts Discussed in Thread: TLC5941
Hello,
We use the LED driver TLC5941-Q1 for an automotive application (LED display on an automotive dashboard).
First, we made an evaluation board to test the component (one TLC5941-Q1 driving five RGB LEDs). Our µC board is an external board and wiring with TLC5941 are made with ribbon cable.
Until recently the board worked good but for some days we experienced drivers failures, with something like VCC/GND short-circuit. When changing the driver, the board works correctly.
Looking at other e2e topic, I found that we shall not send SPI signals to driver when VCC is not supplied : is it still true (other topic was in 2012)?
If confirmed, we will now ensure to supply VCC before applying SPI signals.
Then, we have another problem : when driver is in error state, the XERR voltage is not 0V (more around 1.2V). In our board, we connected a LED and a 332 ohms resistor between XERR and VCC (+5V). We found this schematics in the TLC5941 evaluation board made by TI (not foundable anymore), leading to a current superior to 10mA, when the max current on XERR pin at low state is indicated to be max 1mA in the datasheet : do you think it can be the reason why XERR voltage is not 0V in error state ? Is it a possible reason for driver failure too ?
Thanks in advance for your help,
Best regards,
Julien