This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53014: Could you tell me about TPS53014(SN1206042) ?

Part Number: TPS53014

Hi, team.

Can I tell you because I got a question about TPS53014?

Voltage of VREG5 is indicated in 5.1V@TYP in the datasheet.

Please also tell me the Minimum and Max values.
※I want to know this information when selection of external MOSFET.

Best regards,

Masumi Sekiguchi

  • The VREG5 is generated by an internal LDO. The input voltage minimum of 4.5 V is less than the typical LDO output voltage. So for VIN less than 6 V, the LDO VREG5 output voltage may be less than 5.1 V. I doubt that there is any data for it, but I can check tomorrow.
  • Thank you for contacting me.

    Why are you discussing about "when VIN = 4.5V"?

    Because it is described in the datasheet as below,
    is not MIN / MAX determined by the Individual difference of chips including Line Regulation of 6V <VIN <28V?

    First of all, what we want to know is the MIN / MAX value for 5.1 V @ TYP during normal operation.

    Best regards,
    Masumi Sekiguchi
  • How is this situation?
  • I found the following simulation data:
                                                                                      
    VREG5 Output Voltage "IVREG5=0mA,Ta=25℃"

    Vin   Min     Typ    Max

     4.5   4.38    4.40   4.40 
     5.5    5.07    5.12   5.13 
      12    5.09    5.12   5.13 
      28    5.09    5.12   5.13
    There is no measured data that I can find.