Other Parts Discussed in Thread: BQ2002E, BQSTUDIO, BQ34Z100-G1
Hello,
I am running into a problem with Steps 6 and 7 under "When no close Qmax value is known:" on page 2.
I start step 5 and see that the QEN and VOK bits are set and start charging battery. After charging is complete, the FC bit never sets, VOK is cleared and MaxError remains at 100%.
I am using Chem ID 6113, 2ea1900mAh NiMH cells, and a BQ2002E as a charge controller. I see that the battery reaches full charge.
Is it possible that the trickle-charge function on the BQ2002E is causing this issue?
Thanks,
...kevin