have a TPS63002 IC and its circuit is designed for an input range of 3.5V-4.2V. The values of input and output capacitors as well as the inductor were calculated using WEBENCH. The circuit works exactly as intended, however, there is a peculiar problem. When observed on the Oscilloscope, the "Input" signal seems to have ripples whereas the "output" waveform is clean as a whistle. (Pic 1-6). The blue signal is the input signal while the yellow is the output. This behavior is consistent with load resistance values of (1k, 100, 50, 30, 20)(ohms).
The supply signal is smooth when the dc-dc converter circuit is removed and only the supply is viewed.
The design values are:
CIN=10uF
COUT=22uF
Ind=3.3uH ,112MOhm
Why does the supply have ripples in it?
Regards,
Yash Gupte