This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61236P: TPS61236P Light load issue!

Part Number: TPS61236P

  Dear all:

        I used TPS61236P for 3.7-4.3V  to 5V/1A. We test  efficiency  of lignt load  is not meet DATASHEET.  Can you help to solve the problem?We need about 90% efficiency , thanks!

Vin

I(input)

Vout

I(output)

效率%

3.88V

0.03

5.04

0.018

78

4.27V

0.028

5.04

0.018

75.8