Other Parts Discussed in Thread: TIDA-00628, UCC28720
Dear support member,
My customer will use UCC28722.
Althought output voltage is 15V in the TIDA-00628 design,
Is possible with Output voltage 5V, Iout current 1.4A in this design?
Specification condition
Input Voltage:80V AC~240V AC
Output Voltage:5.3V DC
Output Current :1.2A
Non - Isolated
Design number:TIDA-00628
www.ti.com/.../TIDA-00628
Is this design possible?
Best regard.
Bob Lee.