Hey
I want to boost the voltage from a lipo battery to about 5V and i need to draw current wit peaks up to maximum 7A (in normal conditions peaks up to 4A)
Does it make sense to link two or more TPS61236P in parallel in order to increase the current that can be drawn?
Did I do it correctly in the following drawing or can it be done with considerably less components?