Other Parts Discussed in Thread: BQ27621-G1, GPCCHEM
I have used BQ27621-G1 to perform the fuel gauge of the battery of my design. Application is mobile POS.
Ideally, the system should be designed so that the bq27621-G1 is always powered by the battery, even
during system shutdown, but my system is designed that the bq27621-G1 is only powered when mobile is turned on.
The problem is that If mobile is being charged while turned off then turn on mobile, read the battery voltage level incorrectly. (ex:20%-->50%)
Can I fix it in other ways except the power rail? Initialization? If yes, How do we implement it?