Hi,
I am considering a sink circuit using TPS40057.
Operating condition = input 12 V ± 10%, output 2.5 V, output current -1 A (sink only)
Used as power supply for LCD Vcom.
The circuit constants are determined based on the calculation formula of the data sheet.
The phase compensation constant uses the attached Excel sheet.
I would like to ask one question about setting up an excel sheet.
There is "IOUT_max" in the item of the excel sheet.
In the case of sink only, should I input minus 1 A?
Should I enter plus 1A?
Best Regards,TPS40KType III Loop Stability kVenable_sluc263c-071312_test1_20171102.xls