Hi
Is it possible to use it in circuits like images?
and What is the output current accuracy when Duty = 1%?
[specification]
Input Voltage (Logic) : 3.3V
Input Voltage (Power) : 7.5~15V
Load : White LED 6ch
Maximum load current : 20mA
Dimming control : 22kHz PWM
best regards