Other Parts Discussed in Thread: BQ24004, , BQ24005
Dear all,
one of my customer has notice the following discrepancy in the DS which generates confusion:
1) In the datasheet SLUS476F, (bq24004/24005/24006) page 2 states the recommended operating junction temperature range is -40 to 125'C.
In the same datasheet, Package Option Addendum-Page 1 has a column "Op temp", which reads 0 to 70'C for bq24004/bq24006 devices and -20 to 70'C for bq24005 devices.
What is the recommended temperature range over which the ICs are intended to operate? These two sections seem to disagree.
2) It is essential, for safety, not to charge Lithium-ion batteries while the temperature is below 0'C, hence the APG/THERM input.
The APG/THERM input threshold voltage characteristics are only specified down to 0'C.
If the thermistor and IC are both at -20'C, is the IC guaranteed not to charge the battery?
3) What defines the performance of the IC between -40 and 0'C?
regards,
Domenico