So I have the TL 499A and I want to take a samsung limo battery, then use it to create 20V. I tried to follow the guide lines in the data sheet but it basically just says, "connect the circuit shown in figure one, unless specified in the tables shown, and choose a value for Re1. I don't know what I'm doing wrong but I do know what I'm doing so I'm going to list that.
1) Connected a LiPo battery with a 3.8V rating and 4V measured to the Series 2 input of the TL499A dip.
2) Connect the exact same circuit as shown in the diagram, except re1 was a 22k resistor, not a potentiometer.
3) try a bacagillion different combinations to see if I got different results... I didn't really.
Any help would be appreciated. I didn't see an equaition for Vout using the step up configuration so if you have one that would be wonderful as well.