Tool/software: WEBENCH® Design Tools
Hi,
I have a short question about thermal results in Webench.
In a design simulated by Webench they are using an "Effective Power Block Junction-to-Ambient Thermal Resistance" of 20 °C/W whereas the datasheet states 50 °C/W. Is Webench already considering some active cooling?
Results by Webench:
- Pd in M1 = 2.09 W
- R_{\theta JA} = 20 °C/W
- TA = 30 °C
=> Tj = TA + Pd * R_{\theta JA} =71.8 °C (Webench: 72 °C, therefore, the used formula should be correct).
Thanks for your help.
Best regards,
Reto