Other Parts Discussed in Thread: LM36011, LM3642
Dear sir,
I want to generate this kind of waveform.
1.4A last for 2.4s, and than change to 0.86A last for 20s, and than 0A last for 5.5s, and than 0.61A last for 20s. It also needs to repeat.
As figure below. (This current will flow into LED)
Can I using the given GUI to generate this kind of waveform?
Or at least generate a 1.4A current last for 20 seconds.
Can we get sample code for the MSP432?
Or any suggestion method to achieve?
Thanks.