This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76PL455A: Question about Certification

Part Number: BQ76PL455A
Other Parts Discussed in Thread: , BQ77904, BQ77905

Hi Ti.

I has some questions.

I need 28S Battery AFE and I found BQ76PL455A and BQ76PL455A-Q1.

Is these parts have below certifications?

UL1973(Battery Pack Certi)

UL991(H/W Ceriti)

UL1998(S/W Certi)

IEC60730-1

Thanks.

  • Hi SS,

    For a 28s AFE you will need to daisy chain two pl455 devices together.

    My understanding is that the certifications you have mentioned apply at the end product level, and not the semiconductor level.
  • Hi David.

    Thank you for your reply.

    Another question.
    I need the protection IC for OV, UV, Over current, Short current, etc..
    So I found bq77904/5 and I think I will use 6 bq77095 for 28s cells.
    My application is ESS using 28s cells.
    For this application, 2 BQ76PL455 + 6 BQ77905 is best solution?
    Do you have the solution document?