Hello
I have a question about pin 8 of the PTH12060W.
According to the data sheet, if you do not use No.8 pin track, it is said to connect with Vin.
If nothing is connected to Open without connecting No.8 pin to Vin, will it affect the operation?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
I have a question about pin 8 of the PTH12060W.
According to the data sheet, if you do not use No.8 pin track, it is said to connect with Vin.
If nothing is connected to Open without connecting No.8 pin to Vin, will it affect the operation?
Hello Bae:
If the auito track function is not required. It should be connected directly Vin defeating the auto track function. . If the auto track is left floating or open, . the output voltage during initial start-up can have a significant vout over- shoot and can be non-linear until after about 10-20 msec . See below
PTH12060 and PTH120x0 open/ floating Auto track during power up
PTH12060 and PTH120x0 Auto track connected to Vin . Auto track defeated.
Tom
If the auito track function is not required. It should be connected directly Vin defeating the auto track function. . If the auto track is left floating or open, . the output voltage during initial start-up can have a significant vout over- shoot and can be non-linear until after about 10-20 msec . See below
PTH12060 and PTH120x0 open/ floating Auto track during power up
PTH12060 and PTH120x0 Auto track connected to Vin . Auto track defeated.