This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24250C: BQ24250C

Part Number: BQ24250C
Other Parts Discussed in Thread: BQ27532-G1, BQ24250

Hi,

We are using BQ24250C and BQ27532-G1 in our product.

We use Li-ion Battery of 8000mA (4 parallel batteries).

We charge the battery and it get to full charge and then the input current goes down slowly to 0mA.

We start using our product and consume power from battery for few hours. we can charge if we connect external charger and everything looks fine.

After long time, few hours, when we try charging again, the charger is detected by the IC but the charging doen't start.

Only removing the battery helps or depliting the battery to the minimum only then, we can start charging the battery.

We diasble charging timer of 6 hours but still same problem.

I attached the schematic design.

Best regards,

SImoni Yossi.02. Battery Pack.pdf