This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Charger solution

Other Parts Discussed in Thread: BQ51222

Hello,

              Customer use BQ51222  and USB connector two power source. Two power source (BQ51222/USB connector) both input to a charger to charge battery. The output charge current is 250mA for BQ51222 and USB connector and need I2C configuration.  They also request non-Q1 and Q1 charger solution to meet above requirement. Do we have suitable solutions? Thank you.

BR

Patrick

  • Hi Patrick
    Does the charger have two inputs? One for wireless power and one for USB?
    If this is the case then Q1 is not needed and /AD-EN will be open. But AD should be connected to USB input as a way to turn off wireless power when USB is present.