Other Parts Discussed in Thread: BQ77905
Hello,
I have a few questions regarding the CHG pin and OV conditions related to the BQ77905 and the EVM module.
I have used the EVM module to initially test my cell configuration and it works great. I have also tested my personal design and it also works exactly like the EVM module.
I noticed that the CHG pin will be "low" when I'm below the OV threshold of 4.25V (my cells were 4.15V/each). I am unsure as to whether the hysteresis range comes into effect in this scenario (200mV)?
Do my cells actually have to be less than 4.25V-0.2V = 4.05V before CHG pin will be "high"? What is the reasoning for such a large hysteresis range if this is the case?
Kind regards,