Other Parts Discussed in Thread: TPS92075
Hello,
I have a doubt regarding the "Hold Current" circuit in the phase dimmable PFC flyback controller: LM3447 (or any similar phase dimmable PFC flyback controllers).
Datasheet says that the controller operates in DCM. So when the primary switch (MOSFET) turns OFF, the input current (current drawn from the mains) goes to zero. So if used with a phase dimmer, this would result in zero current through the triac (inside the dimmer) and would lead to turn-OFF of the triac and hence misfiring; unless the "Hold Current" circuit inside the LM3447 gets activated and draws the holding current.
So my question is whether the "Hold Current" circuit gets activated in every PWM cycle? If not, then how the holding current is maintained from the mains when the primary switch turns-OFF?
Regards,
Mathews