This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25895: QC3.0 Both at input and output

Part Number: BQ25895
Other Parts Discussed in Thread: BQ25898D, BQ25890H, BQ25703A, BQ25703, BQ25890

Hi

I am designing a circuit that supports QC3.0 both at input side for charging the battery and at the output side to supply power to supported mobile phones. I am confused on which part to select at input side and want to know how to supply 9V/12V at output side and how to do a handshake with the mobile phone that supports QC3.0. Here are my questions:

1. I see that TI is recommending BQ25890H/BQ25898D instead on BQ25895 for QC3.0. What's the reason for the same? Can BQ25895not support QC3.0? I see that one PowerBank manufacturer uses BQ25895 to enable quick charge. Here is the teardown of the product that uses BQ25895. Link

2. One of the TI Engineers recommended BQ25703A in this E2E thread. I also need Fuel Gauge in my design, which is inbuilt in BQ25703. Which part do you recommend on using? BQ25703 or BQ25890H or BQ25895?

3. I do not know how to enable QC3.0 on the output side(To phones). It'd be great if you can tell me how to do the handshake with mobile and how to support multiple voltages: 5V,9V,12V, etc., Does TI has any part to do this? Or do I have to use multiple boost converters?

Thanks in advance.

Teja