I have a DCH010505S which is supposed to be a 5v to 5v isolated converter. If I put 5v into it it gives 7.6v output. Whatever the input voltage the output is always about 2.5v above. What is happening? I have two of these and they are both the same.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a DCH010505S which is supposed to be a 5v to 5v isolated converter. If I put 5v into it it gives 7.6v output. Whatever the input voltage the output is always about 2.5v above. What is happening? I have two of these and they are both the same.
Tim :
DCH010505 output voltage is dependent upon output load. Product Data sheet Load versus load regulation is below.
Attached is one method to limit the output voltage to 5.6 to 5.1 V range .
Tom