Hi,
I have another question. If we want to replace the LMZ31704RVQT with another module with the following:
Vin (low) = 3.5V
Vin (high) = 7V
Vout = 1.0V
Iout (max) = 3A
Iout (nom) = 1.5A
Is there another module similar to the LMZ31704RVQT that can will work with our criteria?
Thanks,
David