This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MOSFET selection HELP

Hi all,

I need a little help to select an appropriate MOSFET for a four-channel DC/DC converter.

The main requirements are the following:

- f_s switching frequency 50kHz-100kHz

- relatively low R_DSon resistance

- power rating: max. 100 W

- input voltage of the converter: 90 V - 200 V

- output voltages (4 channels): each of them 2-20 V

- maximal I_D (peak current): 10 A

Thank you in advance!