This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62142: Problem with output voltage regulation

Part Number: TPS62142

Hello,

I'm using a TPS62142 in order to provide 3.3V for a TI Lauchpad board and a custom logic board (max. load1.5A) from a 9.9V LiFePO battery. On the power supply board there's also a boost converter with an output voltage of 12V. My problem is that, when i connect the battery (~9.8V) the IC doesn't regulate the 3.3V at the output but ~0.228V. For the design i took as a reference the one given by the webench tool. What could be the problem? Thanks in advance!

Here are the schematic and pcb i'm using and the webench report. 3302.TPS62142_3V3.pdf