Other Parts Discussed in Thread: BQ25505, BQ25570, BQ24210
Charging a single Li-Ion cell 3.7V at 2200 mAh
AC adapter input = 16V at 4A max, 440 mA fast charge, adapter connected as needed
Solar cell input = 16V at 44 mA, slower charge, always connected, always voltage out unless dark
AC adapter and solar cells wired in parallel
Questions
1. Is this IC smart enough to deal with these two inputs?
2. There is a 10:1 difference in output current from the two inputs, can the IC deal with that?