Other Parts Discussed in Thread: BQ34110
We recently purchased the BQ34110EVM-796 with a view to evaluating it on our battery packs.
It appears that the eval board only accepts a cell voltage to a maximum of 48V. The BQ34110 device looks good to 65V.
Why is there a discrepency between the two maximum voltages? When we charge our cells we can see voltages upto 57V so i don't want to run the eval board in our system without some guidance as to what i need to do to ensure its safe.
Also, the datasheet mentions scaling to allow the capacity and currents measured to be extended, but i don't see any further reference to scaling. Is there any further information on the scalling required?