This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2492: Negative voltage tolerance at any pin

Part Number: TPS2492

Hi, Team,

 

Our customer is working on TPS2492, and has troubles for the negative voltage against serge test.

In their serge test, OUT pin is likely to have -1.3V, while their circuit has a varistor.

The DS describes in "Output Clamp Diode" in page 27 that "The OUT pin can withstand a short transient to -1V".

 

Then they have following questions;

(1) The time for -1V short transient ? (<-- no definition for the time)

(2) Judgement criteria where you permitted the "-1V" ?

(3) Could you share any data with -1.0V, -1.1V, -1.2V, -1.3V and so on if you have ?

(4) Can you allow to put Diode at GND pin in order to prevent any reverse voltage.

 

Thanks and Regards,

Metropolitan (Tokyo) Area FAE  Kenji Ninagawa

  • Kenji,

    The OUT pin has a diode for ESD protection that can be damaged with too much energy (it is specified for HBM 2kv JEDED standard). It will start to conduct at > -0.7v. The ABS Max table lists -0.3v with no time constraint. Consider that a steady state value. We know OUT can exceed -0.3v for short periods of time (as in fault protection transients at very high load current) as long as the current is limited above -0.7v due to some output Z (R, and L) and the bypass current into the Schottky. We have tested in the lab with output Schottkys (large with Vf ~ 1v at very high current) and have had no issues during fault testing. Neither have customers. We recognize that it is almost not possible to clamp to -0.3v we have specfied in the abs max table, hence the statement in the DS mentioning -1v but recognize that current cannot be infinate. It is best to have a very strong output Schottky to clamp <1v where the diode current will be limited to safe levels by its own characteristics. These durations are typically <10usec.

    Brian
  • Thanks for the reply.
    The customer was convinced by the explanation.

    Then the customer has one more inquiry.

    He wants the maximum power dissipation of the internal ESD diode as a judgement criteria in case a waveform is over -1V.

    Kenji
  • Kenji,

    There isn't a power specification. It is specified to withstand the ESD energy per the HBM 2kv, 500v per CDM. At 0.3v, forward conduction should be almost 0 so it can take that indefinately.

    Brian