Other Parts Discussed in Thread: TPS61170, TPS61022
Hi,
We got a question from the customer about TPS61081.
Could you help us?
[Question]
They are considering using TPS61081 under the following condition.
Vin=3.0V to 4.3V(1cell Li-ion) or 4.7V(ADP)
Vout=4.5V
Iout=30mA(typ),500mA(peak)
L=4.7uH
- They need non pulse skip operation at this condition. How much is the minimum ON time of this device? They are thinking 4.3V input voltage is tough condition.
- If the input voltage is from ADP, they need pass-through operation(the output voltage follows input voltage). Can the IC operate pass-through operation?
Best Regards,
tateo