This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC08200 Working current is too large,In this circuit,where was broken?

Other Parts Discussed in Thread: ADC08200

I use an ADC08200 to detection the voltage.In the following circuit,it work in 100MHz.Working current 1A.If I break the CLK foot, the current is normal, even on the CLK foot, the working current can reach 1A, obviously abnormal.

  • Hi User5214492,

    I am not certain of what is meant by "CLK foot". Do you mean the current remains the same even when the clock signal is removed from the ADC?

    Can you please provide a schematic?

    Best Regards,

    Dan