Hi,
I'd like to verify the input current for TPS61093:
Test condition as below:
Vin = 3.3V
Vout = 5V
Iout = 0.8A
I tried used WEBENCH to simulate the above test condition by setting the Iout 0.3A (0.8A exceeded the switching current limit) , the average Iin obtained was ~0.67A
Could you help to advise if this is correct way to check the input current?
Hope to hear from you soon
Thanks