Other Parts Discussed in Thread: UCC27611, SN74LVC2G14
I am trying to drive the UCC27611 part with a square wave oscillator but it does not appear to be working. I have attached a document with 4 plots that describe what I am getting.
FET driver and Osc interface.docx
Plot 1 is the output of the oscillator when it is not in the circuit, note that the oscillator appears to have some inherent frequency content superimposed on the square wave. The oscillator is operating at ~4MHz, the superimposed frequency is about 20MHz.
Plot 2 is the output of the oscillator after I connect the output of the oscillator to the input of the UCC27611 part. Note that the shape of the signal is very similar.
Plot 3 is the same as Plot 2 but with the addition of the output of the UCC27611 part past the OUTH and OUTL resistors (blue trace). Note that the output appears to roughly follow the input and it is not a very nice looking square form. I was surprised that the UCC27611 part was not sharpening up the output pulse.
Plot 4 now adds the output of the GaN FET (green trace). I am wanting the FET to switch between 9V (when off) and 0V (when on). Clearly this is not happening.
I am not sure how to proceed, perhaps I just need an oscillator that has a little cleaner output?
FYI, I also have an open question on the forum related to request for a Spice model of an inverting buffer (SN74LVC2G14), I thought I better mention this to avoid confusion.
Also, if you have a recommended Ti oscillator that would work better than the one I am using, I would appreciate knowing about it. At this point, for proof of concept, any frequency from 1MHz to 100MHz would work. It would also be helpful if the oscillator had a spice model.
Thanks for your help
Marc