This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD3138CC64EVM-030: UCD3138EVM and startup problem of Fusion Digital Power Studio

Part Number: UCD3138CC64EVM-030
Other Parts Discussed in Thread: UCD3138PSFBEVM-027, UCD3138

Hi,

I'm testing the Eval-Board UCD3138CC64EVM-030 together with UCD3138PSFBEVM-027,  and I had a problem to startup the Fusion Digital Power Studio(GUI).

At the beginning it worked fine. However, for the second time, the GUI failed to connect the EVM-Board, and  this alert appeared, where the second part in Chinese means: Target of an invocation that caused an exception.

I found this problem was solved in the post "UCD9224EVM and startup problem of the Fusion Design GUI" (e2e.ti.com/.../188586

But I tried to do as showed in the post, and it did not work.

I got the following information:

When using the Firmware & configuration  Download Tool, the following error appeared.  Is the the configuration file not fit for the UCD3138? or any other problems?

Please help me with some advice, thanks!

Greetings,

Longqi