I persuade my customer to use TPS3600D33 to replace MAX793. The schematic is as belows.
But When V330 is power off , TPS3600 switch over to the battery (CR2450), customer found the battery will run out
in about two days. while MAX793 has no this problem , the battery can run up to several weeks.
Could you help check if anything wrong about this schematics? Thank you .
Note: 1. R419 is NC
2. PIN 6/7/8/9 is unused
3. pin 12 is connected with one jumper, but jumper_1 and jumper_2 is not connected.
In other words, Pin 12 is floating.