Other Parts Discussed in Thread: TINA-TI
While looking for a solution for a 12V in (nominal) 7.5V@2A out DC/DC, I found this part. Compared with some other I tried before it on Webench and TINA-TI, this one offers an excellent transient response.
The simulations on TINA raised the following questions:
1- The startup has an inflexion on Vout at 1.5 ms (nominal soft-start time is 1.9ms). That makes startup to extend beyond the nominal. Is it normal? Note: if you extrapolate the initial part of the output voltage before the inflextion, the startup time is around the nominal.
2- I need low ripple and as stable an outuput as possible. Besides the design requires many capacitors and I used 400uF to simulate the supply. This capacitance is the very reason I needed to increase the soft-start time as the converter would not start properly with Webench default setting (0.6ms). The simulation shows a good transient response (~40mV for a 1.8A step, L2=100nF, Cout=400uF) and it stabilizes quickly. Also the high frequency ripple after the 0.1nH inductance is pretty low. So I would like to check I may rely on the simulations results to make the decision about using this part for this DC/DC converter.
I am attaching the TINA-TI file I used to simulate the transient behavior.