This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2057C: Why STAT pin is low level when reinsert battery to charger

Part Number: BQ2057C


Hi,

I have designed a chager using BQ2057C. The battery and charger is separate. When i need recharge the battery, i found the LED is off but there is charge current.

Reappear process:

1. Charge the battery to full and the LED turn off(charge current drop to 0)

2. Discharge the battery until the voltage drop to 4V and there is no battery connenct to the charger.

3. Reinsert battery to charger. There is charge current but the LED is off. Why?

PS:

1. If I doesn't turn off the Vin, when plug and unplug the battery, the LED is off.

2. If I turn off the Vin, reinsert battery to charger. The LED is on.

Could you help to explain the phenomenon and advise how to accomplish LED is on when plug and unplug the battery under Vin.

Thanks

Walsh