Other Parts Discussed in Thread: UCD7242
Hi Liu Jian,
The customer is using UCD9244+UCD7242 for C6000 DSP. Need your support for FUSION configuration.
SYSTEM POWER _ POWER_DSP_CORE.pdf
UCD9244 and 7242 for 6678 OUTPUT 1.xml
There are four output rails. With the attached UCD9244 and 7242 for 6678 OUTPUT1.xml, the output rails of DSP0 1V0 and DSP0 Vcore (=1V) are fine. However, DSP1 1V0 and DSP1 Vcore are always zero. With the attached UCD9244For6678 FOUR 1.0.xml, there is a little improvement. DSP0 1V0, DSP0 Vcore and DSP1 Vcore are fine. But, DSP1 1V0 is zero. I don’t understand why DSP1 Vcore is fine at this configuration. We need your support for,
- Could you pls provide a FUSION design? The schematics are included in the attachment;
- Could you pls tell us the mistake in our FUSION design?
Thanks very much.
Below is the part number of output inductor and capacitor.
L28,L29,L30,L31 |
HM72B-06R47LFTR13 |
0.47uH |
HM72 |
4 |
C1891,C1892,C1893,C1894,C1895,C1896,C1918,C1919,C1920,C1921,C1922,C1923 |
T520D337M006ATE025 |
330uF |
7343 |
35 |
C1889,C1890,C1897,C1898,C1916,C1917,C1924,C1925,C2025,C2026,C2049 |
T55B227M004C0035 |
220uF |
C_2P_114_138X118 |
11 |
C88,C225,C226,C227,C503,C504,C505,C791,C809,C878,C886,C887,C888,C889,C939,C940, |
JMK212BBJ476MG-T |
47uF |
C0805 |
46 |
C402,C408,C416,C418,C430,C815,C816,C1079,C1094,C1096,C1102,C1830,C1884,C1885,C1886,C1901,C1902, |
GRM21BR60J226ME39L |
22uF |
C0805 |
24 |