Other Parts Discussed in Thread: PMP21098, UCC256304, UCC24610
1.UCC28056 (PFC) and UCC25630(LLC DC/DC) are used in the schematic of the design PMP21098.
Now my idea is that: first the supply voltage of UCC28056 becomes Hi, and then UCC256304 works.
But it seems that supply VCC of UCC28056 is provided by PIN12(RVCC) of UCC256304. So if UCC256304 does not work, there is no RVCC to make UCC28056 works.
Did I make a mistake?
Could you help me to find where VCC of UCC28056 comes from?
2. Two UCC24610 is used in PMP21098. Can I replace it with just one TI's IC which can drive two GATEs?
(I have tried to search but nothing found.)
Thank you.