Hello,
The datasheet for the LM22678 recommends to use the -ADJ version for voltages <5V, but to use the 5V for output voltages of 5V and greater. On page 14 it provides information about selecting proper resistances for the feedback node, and it says that "a maximum of 2k is recommended for the -5.0 option". This leads me to believe that Rfbt + Rfbb should equal 2k.
Then I was looking at the SIMPLE SWITCHER Design guide on page 12 (labelled 21) and it recommends values 1k and 8.45k for and output voltage of 12V.
Which of these conditions holds more true? Should I use the resistors suggested in the design guide with the -ADJ version? With the -5.0 version? Or should I use the -ADJ version and use resistors that sum to 2k?
Thanks,
Josh