Our customer consider to use LM46002-Q1 for following inverting circuit.
VIN:5V or 10V
Vout:-17V
Iout:200mA
Fsync:460kHz-480kHz
But they don't like PFM mode of this device.
So they consider to add dummy resister to Load to prevent to enter PFM mode.
Do you have equation of current to enter PFM mode ?
They would like to know the equation or current value to decide dummy resister value.