Part Number: LM340-MIL
I am looking for some clarification on the pin layout of the TO3 package. Per the datasheet pin 1 is input, pin 2 is ground, pin 3 is output, and case is either ground or output. Also in the datasheet in the Pin Configuration and Functions section, the TO3 diagram shows output and input as a pin and the ground being the case. It seems like Input and Output are pins and the case is ground for the TO3 package. What is the actual configuration?