Part Number: UCC28881EVM-680
Other Parts Discussed in Thread: LM25007, UCC28881,
Hi,
I'm designing a power supply that should deliver 3.3V and 5V from 230VAC. The current rating is 300mA @ 3.3V and 100 mA @ 5V (Maximum values).
My biggest concern is that i have a small area to design my board, so i have to make my design similar to the UCC28881EVM-680 power supply board and the DC-DC buck regulator LM25007 like this one http://www.ti.com/lit/ug/snva152a/snva152a.pdf,
So the idea is convert the 230VAC using the UCC28881 in order to obtain 13VDC/225mA which is equal to a power of 2.9W, and then i have to use another DC-DC buck regulator to drop down the 13V to 5V using the LM25007.
I can't use a linear regulator otherwise i can't obtaint the 400mA current to feed the 5V and 3.3V components.
The 400mA needed from ther 5V is divided in two part, the first 100mA will feed the 5V circuit and the 300mA will feed a 3.3V regulator in order to obtain 3.3V 300mA.
1/ i want to know if the idea/schema is correct ? Can the output of the UCC28881EVM-680 feed correctly the LM25007 DC-DC converter ?
2/ as i told in the begining that i have small area to design my power supply, so i have to revise some components size from the UCC28881EVM-680 and i want to know if it still correct.
2-a/ the capacitors :
both input capacitors C1 and C2 'EEUED2W100' in the design are too big so i change them to this capacitors 860241375002 which is thinner. they have the same capacitance as the one in the design but the rated voltage of the new one that is only 400V compared to 450v form the design.
I think 400 is good enough for 230VAC ?
About the output capacitor C5 'EEU-FM1V331L' i change it for this smaller one '25SEPF330M'.
It has the same capacitance but with lower voltage, Only 25V. I think is enough for the output voltage that can climb to 16V ?
and the new one has a smaller ESR 'equivalent series resistance' only 14 mohm compared to the original one which is 30mohm. So this is a good things knowing that the lower ESR the lower the voltage output ripple ?
i want to know if i can lower the capacitance of both input/output capacitors? if yes, how much can i decrease ?
3-b/ inductors :
input inductor L1 ; i changed the 5800-102-RC model with this one ELC09D102F.
output inductor L2; i want to know why the current satruation is chosen as 400mA knowing that the output max current is 225mA ?
can i choose another one with lower current saturation?
Is one of these are good for this application :
- 744772102 : RMS Current (Irms): 300mA , Saturation Current (Isat): 500mA
or this one DR0608-105L :RMS Current (Irms): 400mA , Saturation Current (Isat): 350mA
3-b/ Fuse :
i want to replace the big resistor used as a fuse with a PPTC Resettable Fuse like this one 'LVR012K' ?
Is the holding current of 120mA is enough ?
Because the maximum input power is 3.581W for 230VAC which is equal to a current of 15mA
3-d/ can i remove the resisor R4 connected to the feedback FB pin of the UCC28881 chip ?
Thanks you,