Other Parts Discussed in Thread: TPS650864, LM2767, TPS61040
Hi,
I have the following question:
-if you have on the board a stable 5V can you use to power both the device thru DRV5_1_6 and the external mosfets?
-or do we need to use Vsys for external mosfets?
-what is the function of Vsys if you can power everything at 5V?
In the datasheet there are diagrams with Vsys=4.5V, that is below the min voltage.
Thanks
Umberto