This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH®工具/ TPS63002: TPS63002 Large starting current

Part Number: TPS63002
Other Parts Discussed in Thread: TPS63000

Tool/software: WEBENCH® Design Tools

Hi All,

I used TPS63002 to design the input voltage 4.75v~5.25v output voltage 5V Current 1 A circuit, the schematic diagram is as follows:

The test diagram is as follows:Output no-load, first to input and then start en, the figure on the current is input current, how to reduce the start-up current, Thanks.