Other Parts Discussed in Thread: BQ78350, BQSTUDIO, EV2400
Hello,
I want to charge my battery with the charging parameters from the BQ78350. I can configurate this parameters with BQSTUDIO. During the charge-configuration the BQ78350 is connected to the software (to the PC).
The charging parameters will be saved in the BQ78350. So, everytime I want to charge the battery, the BQ78350 knows, what the charging paramters are.
This means: I have to configurate the charging parameters to the BQ78350 only once. Every other time, when I want to charge, the BQ78350 will already know, with which values (charging-current, charging-voltage, pre-charge-current and so on) the IC should provide the informations to the charging IC.
So BQSTUDIO dont have to be connected everytime I want to charge
Is the way Im thinking correct?